Part Number: DP83867IS
Hi,
In our design DP83867IS used as an SGMII configuration, In the case of SGMII configuration, we need to get the recovery clock of 125MHz from the CLK_OUT pin. Is this possible? also please mention the configuration setting
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IS
Hi,
In our design DP83867IS used as an SGMII configuration, In the case of SGMII configuration, we need to get the recovery clock of 125MHz from the CLK_OUT pin. Is this possible? also please mention the configuration setting
Hi Ibrahim,
Yes, it is possible to output the 125MHz recovered clock to the CLK_OUT pin. You can do this by setting register 0x0170 equal to 0x0010. Since register 0x0170 is part of the extended register set, you will have to use the sequence described in section 8.4.2.1.8 of the datasheet, also listed here:
1. Write register 0x0D to value 0x001F.
2. Write register 0x0E to value 0x0170
3. Write register 0x0D to value 0x401F.
4. Write register 0x0E to value 0x0010.
Section 8.3.3 of the datasheet describes the other possible configurations of the CLK_OUT pin.
Thanks,
David