Part Number: XIO2001
Hi Team,
A Japanese customer request me to post this thread.
the issue as below.
↓
XIO2001 is used on Dell OPtiplex7080,
When I am using PCI bus, the expansion board disappears.
※ PCI to PCI bridge disappeared from the device manager.
Is there any way to solve this problem?
I checked scpz008b pdf
"XIO2001 PCI Express to PCI Bus Translation Bridge Silicon Errata"
I have some questions about 4 ※ in this document.
※TLP transfer may halt when ASPM L0s is enabled on the chipset and the XIO2001.
Will the device manager on the PC disappear after XIO2001 stops?
As the Workaround mentions,
Disabling ASPM L0s on either or both the chipset and XIO2001 will prevent the problem from occurring.
does it mean ASPM should be set to disable in BIOS?
If there is anything else to change, please let me know.
Thanks.
Regards,