Part Number: DP83867E
Dear TI support,
during our development of a cable diagnostic software using DP83867E's TDR features, we've encountered a problem when testing C and D Ethernet pairs -- the 1000BASE-T additional pairs.
When two DP83867E's copper media sides are connected via 1000BASE-T (4 pair) cable, the problem manifests as pairs C and D being reported as "open cable", i.e. there are reflections on the pairs as in the case the cable is opened and not terminated. Pairs A and B are terminated (no reflections).
We have another 3rd party PHY capable of doing TDR. Also the 3rd party PHY reports pairs C and D as being "opened", when DP83867E is used as the link peer.
From the observation, a question about DP83867E's integrated MDI termination rises:
When does DP83867E activate the MDI termination on specific pairs and how to configure DP83867E to act as a proper link partner for TDR (to remain silent but with active MDI termination on all pairs)?
Our observation (please confirm or decline)
1) When DP83867E is powered down by BMCR register, MDI termination on all pairs is disconnected.
2) When DP83867E is in auto-negotiation stage, MDI termination is active on pairs A and B (used for the auto-negotiation) and we are able to use TDR against the DP83867E. The pairs C and D are still un-terminated in this stage.
3) When DP83867E is in active 1000BASE-T mode (Ethernet link is up), TDR is not possible.
4) When PORT_MIRROR_EN is set to 1 in CFG4 register, C and D pairs become terminated, A and B pairs become un-terminated (when DP83867E is in auto-negotiation stage without an active link partner).
Thank You.