Part Number: TLK110
Hello,
About Software Strapping Mode
According to section 3.8 on datasheet, it is described about Software Strapping Mode following.
“There are 3 Software Strapping control registers: SWSCR1 (0x0009), SWSCR2 (0x000A) and
SWSCR3(0x000B) contain the configuration bits used as strapping options or virtual strapping pins during
HW Reset or Power-Up.”
In this case, when virtual strapping pins have already been configured, which value will be reflected as SWSCR1/2/3 registers?
(Configured strapping option values on these registers or configured virtual strapping pins?)
When default values of SWSCR1/2/3 registers will be used, do we need to configure(write) these SWSCR1/2/3 register values ?

Regards,
Tao_2199