This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG720S-Q1: TDR testing

Genius 17425 points

Part Number: DP83TG720S-Q1

Hi all

My customer has below questions, please review and comment.

Best regards

Ueli

------------------------------------

We are preparing for compliance testing of the 1000BASE-T1 interface and for this we need to support cable diagnostics.

We tried running the TDR according to the procedure in “snla371a-Configuring for Open Alliance Specification.pdf” and if we connect no cable to the DUT connector we get as result in register TDR_TC12 (0x30F) = 0x71 which means according to Table 7-1 in the datasheet “Cable OK”.

If we connect a cable with ~1.5m to 2m length we get as result 0x161 which means “Open” and a distance of 1m.

The same behavior can be observed for short circuit conditions directly at the connector vs at the cable end.

 

  

Thus I have 2 questions:

  • Is there some kind of minimum cable length (1m ?) to be connected for the TDR and therefore the cable diagnostics to work properly ?
  • Is the fault distance value (bits [13:8] of 0x30F) in meters ? à minimum detection distance is 1m ?

 

Many thanks and best regards,