Part Number: TUSB4041I
Hi team,
I’ve got three questions on TUSB4041I GRSTz-pin. Could you kindly take a look below?
Q1:
Section 7.6 of the datasheet state below.

Does it mean when VDD11 is stable 10usec before VDD33, GRSTz assertion is not required?
Q2:
GRSTz-pin is controlled by CPU’s GPIO. Therefore it is in Hi-Z (H-level) during the VDD/VDD33 voltage rising. Is it possible to input 3ms (or longer) L-level pulse after the uboot?
Q3:
When GRSTz-pin is pull-downed and keep in reset state, VDD (1.1V) experienced very large current. Is it expected?
Best regards,
Kurumi