This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: incomplete link of DS90UB960-Q1/DS90UB953-Q1 code of camera serdes debug

Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: DS90UB960-Q1,

I'm FAE from Reference design team, my customer Semidrive meets some problems in debug DS90UB960-Q1/DS90UB953-Q1 code of camera serdes.

Customer's question: At present, the init and probe have been completed, and the system has also powered on the camera, some channels are linked, but some channels are not linked. The powered-on sequence of the 960 is also correct. I would like to ask if the camera will be linked as long as it is powered on?? When I encounter this kind of incomplete link, do I need to configure something else?

I have problem upload the c.files sent by the customer in e2e. Can you contact my email for deeper discussion? So I can send the code to you.

BR,

Daoyan