Part Number: SN75DPHY440SS
Dear Sir or Madam,
What are the possible approaches for galvanically isolating a MIPI camera? This is for a medical application (class 2, not life saving, not life sustaining). I’ve designed galvanic isolation for medical devices a number of times and passes TUV tests, but I’ve never had to isolate a MIPI signal.
The preferred isolation rating is 4kVac, 2x MOPP. 2kVac could work too, but that would constrain the design of the system in other places.
The MIPI cameras which I need to work with have 2 lanes 900 Mbps per lane.
Any suggestion, insight or reference is really appreciated!
Best regards,
- Nick
p.s. Converting MIPI to optical fiber would do it, but I don't know which chipset can do it. Galvanically isolated copper connection would do it too.