Part Number: TPS25750
Hi Team,
I would like to know about Variable Supply setting
---------
[Q1]
Is there an upper limit for setting Variable Supply?
<For example>
OK case: min 11V, max 13 so 12V +/- 1V
NG case: min 5V, max 21V so 12V +/- 7V
---------
[Q2]
Can " Fixed " and " Variable Supply " settings be mixed?
<For example>
PDO1 5V (Fixed)
PDO2 9V (Fixed)
PDO3 11V to 13V (Variable supply)
PDO4 15V (Fixed)
PDO5 20V (Fixed)
---------
[Q3]
Can Variable Supply setting overlap with the voltage of other PDOs?
<For example>
PDO1 5V (Fixed)
PDO2 9V (Fixed)
PDO3 11V to 16V (Variable supply) *16V of PDO3 overlaps with 15V of PD4
PDO4 15V (Fixed)
PDO5 20V (Fixed)
---------
Regards,
Hide