Part Number: TCAN4550-Q1
Dear e2e support,
Could you confirm if there is any way to drive the GPO2 directly from the SPI bus; or can we only configure it through the watchdog or interrupt functions?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN4550-Q1
Dear e2e support,
Could you confirm if there is any way to drive the GPO2 directly from the SPI bus; or can we only configure it through the watchdog or interrupt functions?
Regards,
Hi Sebastien,
Unfortunately, the GPO2 pin can only be used for the configurations available in the GPO2_CONFIG bit field (or used in test modes, which would likely not be helpful here). The GPO state can not be manually driven via a SPI write.
Let me know if you have any more questions.
Regards,
Eric Schott