Part Number: SN65DP159
Hello support team,
My customer uses 1.1V as VDD which is converted from LDO 3.3V, however, their LDO power spec is 0.41W.
On the retimer, the power consumption seems to be P=(3.3-1.1)x0.295=0.649W, which exceeds the LDO power spec.
I want to check that when Vcc=3.3V and VDD=1.1V, would the IDD typically as high as 0.295A?

Thanks for the support,
Dave