Part Number: SN65HVD33
Hi,
Will the device output (Y and Z pin) be 0V when the output current exceeds 250mA (Current limit)?
Or will it be High-Z?
Best Regards,
Nishie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD33
Hi,
Will the device output (Y and Z pin) be 0V when the output current exceeds 250mA (Current limit)?
Or will it be High-Z?
Best Regards,
Nishie
Hi Nishie,
The output short circuit current isn't a limit - it is a tested and measured value. If Y and Z are shorted together the worst case scenario is that +/-250mA will flow between Y and Z. Essentially this test is seeing what happens if Y and Z are being driven and the Y and Z lines short circuit - and across this device's operating range the worst you can expect is a current with magnitude 250mA.
However we recommend during normal operation that the output current stays with the range of -60mA to 60mA .
While there is not "max" current listed for the driver on the abs max table - what is denoted is the max rec. junction temperature of the device --> the output current will directly increase junction temperature and depending on environment and how the part is being used the junction could get too hot - this is specified as there are multiple factors at play but its not recommended to go above the -60mA to 60mA under normal conditions.
Please let me know if you have any other questions!
Best,
Parker Dodson