Part Number: DP83867IR
DP83867IRRGZR Ethernet PHY part we are using in our design.
But unfortunately IO requirements violating.
Our SoC supports Max. 1V8 only but PHY side its violating as shown below.

Can you please help us to resolve this..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IR
DP83867IRRGZR Ethernet PHY part we are using in our design.
But unfortunately IO requirements violating.
Our SoC supports Max. 1V8 only but PHY side its violating as shown below.

Can you please help us to resolve this..
Hi Chethana,
May I asked what current level is the VOL for your SoC?
--
Regards,
Hillman Lin
Hi Hillman,

Current level and VOL level for the SoC is shown above.

This is the violation.
Thanks & Regards,
Chethana
Hi Chethana,
We have a driver with a high input impedance on the PHY side, so we do not expect the I(oL) should be this big. The load current should be in the microampere range instead of milliampere range.
--
Regards,
Hillman Lin
Hi Hilman,
SoC side IOL can be set to 2mA only.
What can be done to resolve this issue?
Is there any alternative way??
Thanks Hilman
Hi Hilman,
Is there any formula to calculate VIL for the Ethernet PHY(DP83867IRRGZR )?
Regards,
Chethana
Hi Chethana,
I look at your SoC specification, they provide the VoL with 8mA output current. Could you double check with the SoC for a lower output current situation for VoL? Our PHY only have microampere current leakage.
--
Regards,
Hillman Lin
Hi Hilman,
If we can set the SoC low level output current (IOL) in micro amps, How you can resolve the above issue?
Is there any formula to calculate the VIL of Ethernet PHY?
Thanks & Regards,
Chethana
Adding to the above enquiry,
What IO standard does the TX and RX line of RGMII interface support for all 1V8,2V5 and 3V3 levels.
Hi Chethana,
I am not sure if I understand your problem correctly. Here are the answers for your questions:
--
Regards,
Hillman Lin
Thanks Hilman,
We will check with SoC side and will get back to you soon.
Thanks & Regards,
Chethana
Hi Chethana,
I just want to modify on what I said earlier. Our PHY normally have a leakage current in Microampere and the IEEE standard are in 2mA for the IoL. That is why I want to know what VoL for the SoC when the IoL is in 2mA.
Please let me know if you have more question.
--
Regards,
Hillman Lin
Hi Hilman,
This is what we got from our SOC vendor,
1) Setting IOL to a certain value does not change the VOL , With a lower drive strength, signal will take simply take more time to reach the required voltage level.
2) The IOL = 8mA at the SoC side is the maximum value that you can choose in the tool. You can definitely and should set the current strength as per the end device requirement.
So what we can conclude?
Any suggestion from your end?
Best Regards,
Chethana
Hi Chethana,
If we do not get the confirmation that VOL will get smaller with lower value of IoL (2mA) in the SoC, there will be a mismatch between PHY and SOC specification. We cannot sign off for this one.
--
Sincerely,
Hillman Lin