Part Number: TUSB8020B
Hi
could you help check the TUSB8020B schematic and any need to adjust ?
Thanks you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8020B
Hi
could you help check the TUSB8020B schematic and any need to adjust ?
Thanks you
Hi,
TUSB8020B is not ideal/complaint for bus powered applications. The TUSB8020B will always report as a self powered hub in its descriptors and it exceeds the suspend mode power consumption required by a bus powered device. Functionally this design can work (with consideration to the below comments) since most USB host ports provide extra power. Please note that a compliant bus powered hub application would necessarily limit the power available to the attached downstream devices to prevent the power consumption from the host port from exceeding 900 mA / 500 mA total for both the hub and the devices combined.
I don't think the TUSB8020B is a good fit for this application. What is the main reasoning for using a USB hub here for only one port? It is not a compliant bus powered hub and it would add in considerable power consumption to your application if bus powered.