Part Number: TUSB2036
I am attempting to use the TUSB2036 in a system which requires the ability to boot from a USB flash drive. In the prototype, the hub is recognized by the USB host, but the hub's downstream ports are not powered and downstream connected devices are not recognized. The hub appears to function properly when connected to a PC running Windows 10.
The power supply is stable, the 6MHz crystal is stable and properly oscillating at least 60us before the reset pin is pulled high, and the power supply is stable.
It appears as though the hub is waiting for the proper commands to enable downstream communications and power, because I see USB resets and communications prior to the hub functioning properly on a PC.
What is required for the part to enable downstream communications and power?