Other Parts Discussed in Thread: TUSB8041, TUSB8042, TUSB8042A, TUSB8044AEVM
Hi,
Q1:
Let SMBUSz = 0, how to check if TUSB8041 enter SMBus mode?
Q2:
When SMBUSz = 0, the functions, pin 40 and 42, are assigned to SMBA1 and SMBA2, and we can use these two pins to assign different SMBus address, right?
Q3.
We'd like to know if the register (8h, bit 3:0) is used to enable/disable USB port of TUSB8041
The register 8h can be controlled by SMBus host, not OTP ROM, right?
Q4.
How to let USB HUB to work normally by BIOS FW, can you provide the detailed procedures and steps?