This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994AD: FW request

Part Number: TPS65994AD
Other Parts Discussed in Thread: TIGER

HI Sir,

My platform is Intel TGL-H ,  and  I had two TBT ports with one re-timer on each port.

But now, my TBT  function didn't work. Both ports can source power, but the USB2.0 was work in one port.

Can you give me the correct setting by my design? 

Another question is in the I2C master config setting, there was setting the TBT slave address at 0x40(port 2 was 0x41)

Does this address should meet the platform BIOS setting? Or I need fellow this default is better.

 

Thank You

James