Part Number: ETHERNET-SW
Hi Team,
My Ethernet phy is dp83tg720, it is boot strapped to master mode.
I want to overwrite in software to slave mode. So I write 0x1834 register to 0x8001 for changing it to slave mode. I read back and I see it getting reflected, but I am not able to get the link.
Trying this on TI-PROCESSOR SDK VERSION: 08_01_00_13
1. Should I put in standby ?
2. Should the autonomous bootstrap also changed ?
STEPS FOLLOWED:
1. I write 0x1834 register value to 0x8001 to configure phy in slave mode .
2. For the hard reset ,I write 0x573x register to 0x101 & 0x834 register to 0xc001.
3. For soft reset,I write 0x573x register to 0x001 & 0x056A register to 0x5f41U and checked out,but I couldn't get the link.
I am using CPSW9G SGMII port and DP83TG720 phy ethernet.
Please check and suggest the steps ,which need to be followed or missed out.
Your suggestion will be helpful to proceed further.
Thanks & Regards,
Kaviya M