Part Number: DS90UB960-Q1
Dear team,
In the backchannel direction, SOC will send one register configuration to sensor by serdes I2C pass through function(SOC-->960-->935-->SENSOR). This register value is used to adjust sensor' brightness. The higher the value, the higher the brightness. When they do the ESD system test, they found that sensor will have a change in brightness. They has an assumption that the ESD test impact the communication of the backchannel I2C. For example, SOC send 0x9F to sensor while sensor receives 0x00 which means the register value is changed due to the ESD test.
If above situation happens, can our 960 or 935 detect the I2C error? If so, which register?
Thanks & Best Regards,
Sherry