Part Number: SN65DSI86
Hi team,
Can the SN65DSI86ZQER support 4K/30Hz/8bit color?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
With 4K/30Hz/8bit color, assume pixel clock = 297MHz, 8 bit color = 24bpp
Stream rate = 297 x 24 = 7.128G
Min_DSI_CLK = Stream / (DSI lane x 2)
DSI lane = 8, Min_DSI_CLK = 445.5MHz
So DSI86 will support 4k@30Hz, but you have to use both DSI Channel A and B.
Thanks
David