Hi
because i alway get error message from TI 0xF1 and 0xF6
1.CHA_INVALID_LENGTH_ERR. When the DSI channel A packet processor detects an invalid transmission length
2.DPTL_UNEXPECTED_DATA_ERR. This field is set whenever a data token at in the video stream from DSI was found at an invalid time syntactically
And we had confirm with SOC vendor , they can transfer RGB color format.
Current status is that using TI internal color pattern will display pass. but use SOC to transfer DSI signal without display.
So what can i do to debug this issue.?
We try to bypass TI SN65DSI86 IC and connect to panel is ok.
list is my use command flow
i2cset -fy 2 0x2c 0x5c 0x01 b
i2cset -fy 2 0x2c 0x0d 0x01 b
i2cset -fy 2 0x2c 0xff 0x07 b
i2cset -fy 2 0x2c 0x16 0x01 b
i2cset -fy 2 0x2c 0xff 0x00 b
i2cget -fy 2 0x2c 0x5a
i2cset -fy 2 0x2c 0x0a 0x06 b
i2cset -fy 2 0x2c 0x10 0x26 b
i2cset -fy 2 0x2c 0x12 0x55 b
i2cset -fy 2 0x2c 0x94 0xe0 b
i2cset -fy 2 0x2c 0x0d 0x01 b
i2cset -fy 2 0x2c 0x5a 0x04 b
i2cset -fy 2 0x2c 0x93 0x30 b
i2cget -fy 2 0x2c 0x0a
i2cset -fy 2 0x2c 0x96 0x02 b
i2cset -fy 2 0x2c 0x96 0x0b b
i2cset -fy 2 0x2c 0x20 0x80 b
i2cset -fy 2 0x2c 0x21 0x07 b
i2cset -fy 2 0x2c 0x24 0x38 b
i2cset -fy 2 0x2c 0x25 0x04 b
i2cset -fy 2 0x2c 0x2c 0x2c b
i2cset -fy 2 0x2c 0x2d 0x00 b
i2cset -fy 2 0x2c 0x30 0x05 b
i2cset -fy 2 0x2c 0x31 0x00 b
i2cset -fy 2 0x2c 0x34 0x94 b
i2cset -fy 2 0x2c 0x36 0x24 b
i2cset -fy 2 0x2c 0x38 0x58 b
i2cset -fy 2 0x2c 0x3a 0x04 b
i2cset -fy 2 0x2c 0x5b 0x00 b
i2cset -fy 2 0x2c 0x3c 0x00 b
i2cset -fy 2 0x2c 0x5a 0x0c b
i2cset -fy 2 0x2c 0x59 0x1b b