This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD Protector for LEDs



Hello,

I need a ESD Protector Device which has automotive qualification specification.

I am going to use this ESD Device to protect to LED. 

Technical specifications should be;

VCL clamping Voltage range:  3.7-5V

ESD protection ±30kV Air & Contact discharge

Rdyn dynamic resistance equal or lower than 0.2Ω

Regards,

Mehmet COBAN