Part Number: LMH1208
Dear ,
the LMH1208, Can default register use directly? I did not match the register,so want to confirm it ,tks~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH1208
Dear ,
the LMH1208, Can default register use directly? I did not match the register,so want to confirm it ,tks~
Hi Cooper,
There are some pins - such as SLEW_CTRL, SDI_VOD, ENABLE, HOST_EQ0, and etc - that need to be set correctly. Given these, you should be able to use the part with default register settings. Please refer to the data sheet for these control pins.
Regards,,Nasser