Part Number: DS90UB941AS-Q1
Dear teams,
My customer is using DS90UB941. Could I ask following support need from your side?
1. Coaxial mode is used for Ser & Deser. Has anyone used this mode before?
2. If it works in Coaxial mode, it is necessary to change the MODE configuration and the output port configuration of DOUT0/1. Are there any other points that need to be paid attention to?
3. In LVDS mode, a common mode coil is generally added to the output port. In Coaxial mode, is there no need for a common mode coil?
4. DOUT0/1 – Connect the capacitor and resistor to GND under Coaxial. Do the resistors and capacitors need to be placed close to the chip during PCB Layout?
Thanks!
Dylan