Hello Team,
under which conditions min and max values below are tested?

In your datasheet a min and max value for the propagation delay is given. For example, min-value is 1.4 ns and max-value is 3.6 ns. Where does the difference of (3.6 - 1.4 = ) 2.2 ns come from? Are such differences really to be expected from device-to-device under the same conditions? Or is a smaller difference to be expected between individual devices at the same ambient temperature and same supply voltage and same package? For example, the data sheet does not distinguish between different supply voltages.
If the difference is smaller: What would be the min and max propagation delay value at a supply voltage VCC of 3V3 and package SOT-23 (5)?
Thanks and Best Regards, Hans