Part Number: DP83826E
Hi,
do I understand the datasheet correctly when assuming the following:
Recovered clock can be outputted via LED0 (Pin30) or LED1 (Pin31).
According to datasheet (table 9-76 and 9-77, DS from 02/22) for both I have to set cfg_led0_gpio_ctrl[2:0] = 001b.
When using LED1 as output for recovered clock LED0 can NOT be used for LED anymore? (because cfg_led0_gpio_ctrl[2:0] = 001b ??)
So basically the questions are:
Where (which Pin) and how can I output the recovered clock?
Can I output recovered clock on LED1 AND use LED0 as LED0 (e. g. as LINK OK)?
Why are registers cfg_led0_gpio_ctrl and cfg_led1_gpio_ctrl of type R(ead) ?? I am not a SW guy but I would assume they are at least W(rite)
Thanks
Mathias