Part Number: TPS25868-Q1
Other Parts Discussed in Thread: TPS25858-Q1, TPS25869-Q1
Hi Team,
Does TPS25868-Q1 have reverse current blocking funtion on USB output ports and the internal MOSFETs?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25868-Q1
Other Parts Discussed in Thread: TPS25858-Q1, TPS25869-Q1
Hi Team,
Does TPS25868-Q1 have reverse current blocking funtion on USB output ports and the internal MOSFETs?
Regards,
Hi Kuno,
Got it, thanks.
BTW, I have another question about USB load switch.
My customer needs to desgin for both USB type C and USB type A(support BC1.2), so I think TPS25868-Q1 should be a suitable solution.
However, not like TPS25869-Q1, TPS25858-Q1 doesn't have USB load switch control feature, I am wondering if my cusomter needs additional load switches to control the ON/OFF of USB portA and port B repectively?
Hi Charles,
Yes, you can use the TPS25868-Q1 to meet this requirement, and this device only has a total EN switch indeed, if you pull up this EN, port B will be output 5.1V , for the port A, when it has a Rd in CC pin, it will output 5.1V too, and you do not need to add a additional load switches for controlling the port A and port B.
BR,
Kuno