Part Number: TFP401
Hi all,
in my design, TFP401 is configured so that DFO input pin is Low; this means that ODCK clock runs continuously. When no video input is connected, I measure a frequency of about 1,5 MHz; the problem is that sometime, after a long usage, that frequency drops to about 500hZ. If logic is connected to this clock, like is my case, errors can occur in the elaboration. The question is: is this a known issue? What can cause it? Ho can I solve, other than using the internal oscillator for clocking logic? I think a redesign of the system is more elegant, I want however try to understand what is wrong with current implementation
Best regards
Fabrizio