Part Number: LMH0071
Hello team,
I have a question about RXCLK.
If the output of the signal generator is input to RXIN0 when it is not settled, does it affect the frequency output from RXCLK?
The details of the question are as follows,
Good condition: Input 270 MHz to RXIN0 while the signal generator signal is settling. 27 MHz output from RXCLK is confirmed.
Bad condition: Input while starting up the signal generator, settles to 270MHz in about 3 seconds; RXCLK output is locked at 27.5MHz~28MHz.
Please let me know your opinion.
Regards,
Masakazu