Part Number: DS250DF230
Hi Team,
Could you please help to check what does this comment mean:
(2) The input and output negative-voltage rating may be exceeded if the input and output current ratings are observed.
- I want to known if this requirement relax is only valid for MIN(-0.5V) which could be even lower than -0.5V if the current is very small, like 0.1mA.
- For MAX +6.5V limit, can we use higher voltage Vinput more than 6.5 V connect to component but with very small current, like 0.1mA.

Thanks.
B.R.
Zhizhao