Part Number: TUSB2036
We are working with a DART-MX8M-MINI and the TUSB2036 is connected to two downstream port. the upstream is connected to DART-MX8M-MINI.
But we were forced to switch to a TUSB2036 hub, which is not detecting the devices downstream. We get a cryptic USB error "-71".
We tried switching the NPINTx pins to GND, and adding pull-ups to the OVRCURx/OCPROT pins, but it did not solve the problem.
We didn't use termination resistors, just added 90Ohm common filter. do we have a problem like this error message, because of termination resistor?
Thanks