Other Parts Discussed in Thread: SN75DP149
Hi Ti
I am trying to design a Self Powered Dock station that is connected to a Portable Device.
- USB 2.0(A) 4Ch, USB3.0(C), HDMI, Ethernet
I have configured the system.(Temp)
Question 1) Can I connect to a PC by converting DFP <-> UFP with USB C 2.0 only?
SS line remains connected to SN75DP149
Question 2) Please recommend a USB CC Controller. (in stock)
Question 3) Is it possible to operate USB Alt mode only when HDMI is connected?
Question 4) Is it possible to use the chip without an HDMI license?
Question 5) If there is a better design direction, please let me know.
Sincerely
Jeong