Part Number: TPD6S300
Other Parts Discussed in Thread: TPS65987D, TPS65994AD
If there are no controller, what should we do with CC1/CC2 pin. should i just no connect it?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD6S300
Other Parts Discussed in Thread: TPS65987D, TPS65994AD
If there are no controller, what should we do with CC1/CC2 pin. should i just no connect it?
Thanks
Hello,
Would you be able to give more information on the Type-C port this device is being used in? Specifically why they are wanting to implement a protection device like the TPD6S300 if there is no CC controller?
We just want to use it on a regular type C for the computer without ThunderBolt. From the Intel guideline, the CC1/CC2 connect to the Thunderbolt PD, but we are not using Thunderbolt so no PD is needed. so right now, we only have C_CC1 and C-CC2 connect to the CC1 and CC2 of the USB C.
Hello Binh,
There are other times when a PD controller is needed, not just for Thunderbolt. For example, if you want to support >5V, you will need a USB Type-C PD controller. If you want to support alternate modes like DisplayPort, you will need a USB Type-C PD controller.
If you could share the entire Type-C requirements that would be helpful
Hi Adam.
we only support 5V for USB C. We want to have USB 3.0 speed on USB-C and running DisplayPort in the USB Type-C port too.
is there a reason why we need the PD controller if we running DisplayPort?
Thanks
The DisplayPort negotiation that takes place on a Type-C port occurs between the two PD controllers. So if you would like to support DisplayPort on your Type-C port, you must implement a PD controller. There is really no way around this requirement since the DisplayPort negotiation happens on the CC pins which connect to a Type-C PD controller.
Device that we would recommend to allow for this negotiation is the TPS65987D
This make sense. Just want to confirm, The C_CC1 and C_CC2 of the TDP6S300 will go to the CC1/CC2 of the USB Type C connector. The CC1/CC2 of TDP6S300 will go to the Type-C PD.
Do you recommend other product beside TPS65987D. The problem with TPS65987D is the operating temperature.
We need to operate minimum of -40C-+70C
Would the TPS65994ADRL work?
Thank you
Hello Binh
Just want to confirm, The C_CC1 and C_CC2 of the TDP6S300 will go to the CC1/CC2 of the USB Type C connector. The CC1/CC2 of TDP6S300 will go to the Type-C PD
Yes that is exactly right
For the device recommendation, if you require the lower temp range, then the TPS65994AD would be the correct device to use.