This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL16C750E: Odd behavior of the TX/DTR at startup

Part Number: TL16C750E
Other Parts Discussed in Thread: TL16C750

Hello,

While testing out our design using the TL16C750E, we came into an odd behavior.

We are using the component in RS485 mode so /DTR is our TX_EN and /RX_EN signal for the transceiver connected after the component to connect to the RS485 signal.

Here is what we observed:

  • At reset, the component sets /DTR high and TX high (as stated in the datasheet). Thus the RS485 output is high after the transceiver.
  • After the reset phase, /DTR is kept high the TX output goes low. Thus the RS485 output is low after the transceiver.
  • Once the component is configured in RS485, /DTR is still kept high and the TX output goes back high. Thus the RS485 output is high after the transceiver.
  • After the transmission of a first byte, /DTR goes low, thus putting the RS485 output hi-Z.

I see two problems there:

  • The toggling of TX high/low at the beginning could loose the receiver in front as it looks like a start bit.
  • If the TL16C750 is not master of the bus, then there will be a collision until a first byte is transmitted by the component.

Is this behavior known/as expected ?

I have taken some oscilloscope screenshots below.

This first one shows a long recording, we see the component startup then a long delay before something happens (data exchange from TL16C750 to a CPU) which corresponds to us starting the CPU debugger to configure the part and start communicating.

A zoom of the startup:

A zoom of the behavior at TL16C750 configuration and before data is exchanged first:

A bigger zoom of the behavior after first exchange (bad resolution as we are working on a high time period on the oscilloscope):

Best regards,

Clément