This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI recommendation



Hello:

There are the following switching chip requirements, please help recommend resources and provide specifications, thank you!

1. For USB3.0 to DP chip, refer to ITE8855B, and the performance can be consistent.

2. DP to Mipi chip.

  • Hi,

    I can't find the ITE8855B datasheet on the ITE website, but I did find IT8855FN on their website which says USB PD 3.0 controller *1 or 2 ports or with Alt. mode MUX. We do not have an integrated PD controller + MUX solution. For MUX only solution, please use the TUSB546 or the TUSB1046.

    Unfortunately we do not have a DP to MIPI solution.

    Thanks

    David