This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410: What is the clock of the differential signal outputs?

Part Number: TFP410

Hi team,

1. The input signal customer used is 148.5MHz and configured TFP410 according the datasheet. There is no signal captured by using 500Mhz and 1Ghz bandwidth oscilloscope. Customer wants to know the clock of the differential signal outputs to classify if they use the wrong measure method. Do you have any comment on that?

If the reason is not the oscilloscope, the problem comes from the wrong configuration of the registers.

2. For the CTL_1_MODE register, when power up the chip, what should be written to TDIS and PB if we don't need any function of it?

3. Is the software reset needed when power up to configure the resisters?

4. Do we have a document or tools to guide how to configure the resister?

Thanks a lot

Matthew Chen