Part Number: DP83848Q-Q1
Hello Texas instruments specialists,
I have some weird behavior with DP83848Q-Q1 which I can not understand.
I don't have 50MHz output at Pin "CLK_OUT".
Description:
We use the Pin "X1" to input a 50MHz oscillator clock reference (Signal from a EBRA53T2H-50.000M oscillator).
Furthermore Pin "CLK_OUT" is used as a reference for our MCU.
In most cases this works very well, we have the 50MHz signal output provided and the MCU can be reached via ethernet.
In some cases this "CLK_OUT" output is not given. I have no 50MHz signal output and therefore no connection via ethernet to the MCU.
Examination:
I checked the signals "X1" and "CLK_OUT" with an oscilloscope: 50MHz in, nothing relevant out.
I checked the connection of Pin "MII_MODE": It is connected to 3V3 via 1kOhms Pull-Up.
When I use the 50MHz signal directly from the oscillator instead, everything is working fine.
The only problem is that we do not have the output at "CLK_OUT".
In datasheet "DP83848Q-Q1" it says:
RMII 50 MHz CLOCK OUTPUT: This pin provides a 50 MHz clock output to the system.
For RMII mode, it is not recommended that the system clock out be used as the reference clock to the MAC.
Question:
Is this "CLK_OUT" something I can rely on even though it is 'not recommended' for 50MHz / RMII mode?
If not, why is it working in most cases (approx. 8 out of 10 are functional)?
Under which circumstances there will be no output at this pin?
Hope someone has an answer.
I'm looking forward to hear about that.
Thanks in Advance
Greetings Markus