Part Number: PCA9543A
Other Parts Discussed in Thread: ISO1540, ISO1640
Hello E2E Experts,
Good day.
I have a design that will use two smart battery packs (SMBus) I have looked at the PCA9543AD to communicate with them from the I2C host.
Do I also need to use an isolation device such as the ISO1540DR between the batteries and the PCA9543AD? There will be times when the battery is
connected to the hardware but the hardware will not be on.
Or, does Ti have a product that has both the ability to interface I2C and SMBUS and also isolate the battery bus from the host bus?
Thank you in advance for your support.
Regards,
CSC