Part Number: DP83826I
Hi Experts,
The customer is looking at the datasheet of DP83826 and got a little bit confused about STRAP2 and STRAP7 signals in Basic Mode.
According to "Table 7-1. Pin Functions (BASIC Mode)" the two signals are PD (pull-down) but in "Table 9-14. PHY Address Strap Table" and "Table 9-16. Auto-Negotiation Strap Table" there is information that default state of STARP2, STRAP7 is "1"
Could you explain to me how exactly it is?
Thank you
Regards,
Marvin