Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550,
HI team,
Customer feedback that with below code they got the readData = 0xC3000048, is there any change on the TCAN4550 silicon or driver, which one will be correct?
And these bit 24:26 is reserve in TCAN4550-Q1 datasheet.
The code is copy from radar BU's TIDA02004 reference code
TIDA-020004
void TCan4550_Initialize(void)
{
...
uint32_t opMode = 0xC7000048;
/* disable CLKOUT in 1p0 silicon, enabled by default and causes noise issues on SPI bus */
do
{
AHB_WRITE_B_FL_32(DEV_MODE_PINS, opMode);
readData = AHB_READ_B_FL_32(DEV_MODE_PINS);
System_printf("readData = %x\n", readData);
} while (readData != 0xC7000048);
...
}
Thanks,
Wesley