Part Number: THVD8000
Other Parts Discussed in Thread: THS6222
Hi Team,
The parallel aggregate impedance should be selected so that the total equivalent impedance at the carrier frequency is Z ≥ 375 Ω. This assumes RS-485 loading with 60 Ω termination. If no termination is used in the application, then the total equivalent impedance at the carrier frequency could be reduced to Z ≥ 60 Ω.

Question:
Why the equivalent impedance should bigger than 375ohm with 60 ohm termination RL? How does the 375ohmn comes out? Thanks.