Other Parts Discussed in Thread: TCA6416A, TCA9539
I’ve been reading through a copy of the datasheet (SCPS243 –SEPTEMBER 2012) and I haven’t been able to find the answer to the following question. Could you please answer it or point me to where I can find the answer?
- Is there any way to reset the part without pulling power if the reset pin is not connected to the system master? Perhaps a register to write? Or maybe just writing all zeros to the registers (the default value for all of the non-reserved registers is zero according to the datasheet)?
Are there any high-GPIO count devices that can be reset via the I2C bus (writing to a register)? I looked at the TCA6416A and the TCA9539, and I don't see any register that would control the IC in this manner.
Mark