Other Parts Discussed in Thread: TIDA-050047,
Hi TI engineers,
I have some problem about power path of TPS25750.
I want to build a bi-direction DRD USB type-C(up to 65w) PD + Charger solution, so I refer to TPS25750EVM and TIDA-050047
what puzzles me is there is 5V DCDC connected PP5V and the TIDA-050047 said 'this design uses the PP5V power path to supply a 5 V source and the PPHV power
path to source higher voltages', so in 5V output source application why not output 5V through PPHV bi-direction power path?
I know PP5V also in charge of PPCABLE supply(VCONN), so 5V supply is necessary, my purpose is let PP5V just for PPCABLE use no for VBUS use and replace 5V/3A+ DCDC with a LDO(just need small current capacity) for cost down, can it works? is the 5V DCDC necessary ?
TIDA-050047 list some configuration case in APPLICATION GUI TOOL, It just has the configuration I need, as shown in the blue circle in the figure below:
but when I use the GUI tool, the configuration case which I needs disappeared, why?
Last question, the external device need 5V output, which REG of TPS25750 decide PP5V or PPHV power path output 5V????