This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS31: SN65LVDS31 connect to SNL65LVDT33 over 2.5 meters

Part Number: SN65LVDS31

Dear Sir/Madam,

I want to design a SPI to LVDS connection over 2.5 meters using SN65LVDS31 (Transmit) and SNL65LVDT33 (Receive with internal terminating resistor).

i'm considering fews methods of doing the 2.5 meters inter connection in order to make sure i get the best signal performance and also the smallest connector size.

If I chose to use IDC Flat ribbon cable, can I use 0.635/0.64mm cable pitch? Do Iyou suggest to separate each signal with a Ground or can I separate them as a pair with ground? The idea is to use the smallest connector that I can use?

Do I need to use a Twisted pair IDC Ribbon Cable of either 0.64mm or 1.27mm cable pitch and do direct solder between the 2 boards.

Hope to get some advice. thx

Best Regards,
kpk