This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: Request a guide for DRP dongle

Part Number: TUSB320

Hi, Ti Team

I want to make a Dongle included USB 3.0 1Port, Ethernet 1Port. (Ethernet : USB 2.0 to Ethernet IC)

The problem is that Ethenet must be supported through the USB Hub, but USB C must perform DRP (Dual Role, DFP or UFP) operation.

1. Review the block diagram below
    A.  When (1)* TUSB320DFP Role (USB C connect to OTG Device)
         -    (1)* : ID -> LOW (Open Drain)
         -    (2)* : Keep UFP
         -    (3),(4)* : Switch to 'B'

    B. When (1)* TUSB320 UFP Role (USB C connect to PC)
         -    (1)* : ID -> High (External Pull up)
         -    (2)* : change to DFP
         -    (3),(4)* : Switch to 'A'

2. Are there any precautions when changing USB DFP <-> UFP?

- usb reset?

Sincerely

Jeong