Part Number: TUSB1044
Hi,
In OFF mode, I would like to use the VCC voltage of the TUSB1044 is 0V.
I have two questions.
Q1:When I continue to use the TUSB1044 with VCC=0V, is there damage to the TUSB1044 ?
Q2:When VCC is 0V, are differential signal ports(URX1, DRX1, UTX1, DTX1, URX2, DRX2, UTX2, DTX2) Hi-impedance?
Best Regards