Part Number: DP83TC812S-Q1
Other Parts Discussed in Thread: DP83848K
We are using the above PHY(PHY1) in a back to back configuration with a DP83848K(PHY2). Currently we use the CRS_DV from PHY1 to control the TX_EN of PHY2. Because the CRS_DV is not in sync with the start of the dataframe, we are loosing packets. To fix this we would need to use the RX_DV signal instead of the CRS_DV signal. The datasheet clearly shows this possibility on page 52, Figure 8-15.
I suppose there should be a parameter to configure this in one of the SMI-registers. I was not able to find that parameter though.
Were can I find the configuration bit or pin strap to change from CRS_DV to RX_DV in RMII mode?
Thanks in advance!