Part Number: PCA9306
Hi Team,
As for the datasheet "8.1.2 correct device set up", there are setup examples that connect EN and Vref2 terminals to Vcc2 via 200kΩ resistor, but is there a tolerance range of the 200kΩ? (e.g. recommended for use between 180kΩ and 220kΩ etc.)
In the datasheet setup example, Vcc1 = +1.8V, Vcc2 = +3.3 V, while we use Vcc1 = +3.3V, Vcc2 = +5V condition, do you have the optimum resistance value condition under the conditions of +3.3V and +5V? (voltage gap in setup example is 1.5V(3.3V-1.8V), voltage gap in our condition is 1.7V(5V-3.3V). I think there is no difference between 1.5V and 1.7 V)
Beat Regards,
Tom Liu