Hi team,
Can 947 work normally at the situation of variable Htotal, variable frame rate, fixed PCLK? Thanks!
BR
Jiawei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Can 947 work normally at the situation of variable Htotal, variable frame rate, fixed PCLK? Thanks!
BR
Jiawei
Hello Jiawei,
Yes this can when paired with any FPD III deserializer 92x or 94x.
Note that when using this method with 940 specifically, then the PASS pin will not function correctly but the CSI-2 data flow should be able to work correctly.
Best Regards,
Casey