Part Number: TSER953
Other Parts Discussed in Thread: TDES954, LMK1C1102
Hello,
Is it possible to use the V3 Link TSER953 & TDES954 as both PoC and Data I/O for not only the Serializer and Image Sensor but also an IMU?
All three would live on one board inside the product. The image sensor would use MIPI & I2C Interface, following the standard setup described in the TSER953 data sheets. The IMU MEMS we are looking into has a configurable host interface that supports either I3C, I2C, or SPI serial communication. The PoC would be split between all three components.
Last part to the puzzle . . . What is the potential of one TDES954 receiving data from two different Camera/IMU setups, each having it's own TSER953, Image Sensor, and IMU? Is that overload on a single DES?
I've added a quick line sketch to help describe what I am asking. The use case is for an Augmented Reality system. Thanks!
David